Execute Sequencer
Before executing the sequencer, enable Data Logging if you want to log measurements for the sequencer (see below).
Press
to execute (run) the sequencer.
The execution logs are shown on the Log panel. You can view the information of current status and error messages of the execution from the Log panel.
To manually stop the sequencer, click
.
If data logging is enabled, you can view the data logging progress in the Data Logger view.
Data Logging
Before executing the sequencer, select or clear the Data Logging check box to enable or disable data logging.
When enabled, measurements is logged and readings are stored in a data log on your computer.
For example – C:\Users\<user_name>\Documents\Keysight\PathWaveACSource\Data Logs\.
The data log file name consists of the AC Source model number followed by "DataLog", the date, current time, and a numeric index. For example, AC6906HDataLog-2021-11-20-11-40-26-31.
While not connected to an instrument, you can load a previously-stored Data Log file and view it in the Offline Data Log Viewer. For more information, see Load Offline Data Log.
Monitor Outputs
Monitor measurements outputs without navigating to Instrument View. See Monitor Outputs.